Stulz-ATS Announces Release of the CeilAiR-OHS-OA
January 14, 2010, Frederick, MD - Stulz-ATS announces the launch of its newest addition to the already robust CeilAiR brand of ceiling mounted precision air conditioners: the CeilAiR – 100% Outside Air (OHS-OA).
The CeilAiR-OHS-OA products are available from 4 to 22 tons, ranging from 500 to 3,000 cfm, in six incremental cabinet sizes. The space-saving air conditioners are mounted in the ceiling and provide 100% outside air helping building owners meet ASHRAE 62.1-2007 requirements, improve indoor air quality (IAQ) and combat sick building syndrome. Typical applications include schools and universities, tenant fit-outs, hospitals, labs, and office spaces.
Standard features of the CeilAiR-OHS-OA line include the Stulz-ATS new E2 microprocessor controller, and energy-efficient hot gas reheat to meet more stringent ASHRAE energy usage guidelines and to meet LEED design requirements. Other features include dehumidification mode, to help manage moisture control in the building; dual air filtration to eliminate particulates; and high efficiency forward curved electrically commutated (EC) fans to optimize air flow.
“The addition of the OHS Outside-Air line to our offering represents our dedication to the pursuit of discovering cleaner, more energy efficient methods of cooling for our customers,” says Oliver Stulz, President of Stulz-ATS, “and this gives building owners one more choice of Stulz-ATS products using the EC plug fans.”
Find out more about CeilAiR Ceiling Mounting Air Conditioners